Part Number: TPS767
Hi team,
I have a question about TPS76701.
If the output voltage of TPS76701 is set to 5V
by external resistors,will the dropout voltage be same as TPS76750?
Best regards,
Tsuyoshi Tokumoto
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS767
Hi team,
I have a question about TPS76701.
If the output voltage of TPS76701 is set to 5V
by external resistors,will the dropout voltage be same as TPS76750?
Best regards,
Tsuyoshi Tokumoto
Hey Tsuyoshi,
The drop out voltage of the TPS76701-EP is not specified in the datasheet.
This is due to the note at the bottom of page 7 in the datasheet:
"NOTES: 2. Minimum IN operating voltage is 2.7 V or VO(typ) + 1 V, whichever is greater. Maximum IN voltage 10V"
If the TPS76701-EP is set to 5Vo output, input should be set to 6Vin.
Thanks,
Daniel
Hi Daniel-san,
Thank you very much for your prompt reply.
I understand your answer.
Best regards,
Tsuyoshi Tokumoto