Other Parts Discussed in Thread: SMJ320C6701-SP,
For the SMV320C6727B-SP and SMJ320C6701-SP DSPs, do the power rails need to be sequenced at power-up and/or de-sequenced at power-down?
Thank you,
Rajan.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
For the SMV320C6727B-SP and SMJ320C6701-SP DSPs, do the power rails need to be sequenced at power-up and/or de-sequenced at power-down?
Thank you,
Rajan.
For the C6727B, there is a paragraph in the datasheet regarding this:
4.7.1 Power-Supply Sequencing
This device does not require specific power-up sequencing between the DVDD and CVDD voltage rails;
however, there are some considerations that the system designer should take into account:
1. Neither supply should be powered up for an extended period of time (>1 second) while the other
supply is powered down.
2. The I/O buffers powered from the DVDD rail also require the CVDD rail to be powered up in order to be
controlled; therefore, an I/O pin that is supposed to be 3-stated by default may actually drive
momentarily until the CVDD rail has powered up. Systems should be evaluated to determine if there is
a possibility for contention that needs to be addressed. In most systems where both the DVDD and
CVDD supplies ramp together, as long as CVDD tracks DVDD closely, any contention is also mitigated by
the fact that the CVDD rail would reach its specified operating range well before the DVDD rail has fully
ramped.
Similarly, the C6701 has a shorter, but essentially equivalent paragraph on page 26.
Power-Supply Sequencing
TI DSPs do not require specific power sequencing between the core supply and the I/O supply. However,
systems should be designed to ensure that neither supply is powered up for extended periods of time if the other
supply is below the proper operating voltage.
If this answers your question, please click "This Resolved My Question"
Regards,
Wade