Part Number: AM26LV31E-EP
In an electronic board we are using the AM26LV31E-EP differential line driver.
For the LIGHTNING qualification test, we need to inject a burst of voltage pulses (in both polarities) into the individual outputs of the AM26LV31E-EP (protected with TVS).
The datasheet shown the Vo (Output voltage range) ABSOLUTE MAXIMUM RATINGS (–0.5V / 6V).
What does this parameter represent? Is it the maximum voltage that I can force at the output?
What is the maximum continuous voltage I can force in the driver outputs?
What is the maximum voltage pulse that the driver outputs can withstand (amplitude, duration, duty cycle)?
Thanks and best regards.