Hello,
We are using a ADC10D1000QML for a Front End Application (Input, LNA, DIFF-Amp, ADC) in our EQM Model. During the commissioning, we ascertain a unstable state (Swing with circa 700 MHz) after a self calibration command.
The unstable situation of the Q-Channel is persistent (The swinging signal is not measurable outside the ADC, the swing must be in the ADC or reference pin)
The I-Chanel is 100% healthy and is working well.
Have somebody else the same problem or is there a well known solution available?
Thanks for response.