This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5328-EP: BSDL file

Part Number: MSP430F5328-EP

Hello e2e,

where we can get the BSDL file of MSP430F5328-EP for customer? thanks in advance.

LEON

  • Leon,

    Here is excerpt from the MSP430 JTAG wiki.

    processors.wiki.ti.com/.../JTAG_(MSP430)

    ---

    All MSP430 devices have a JTAG interface for debugging, program development and Flash programming only.

    This User's Guide SLAU265 describes the functions that are required to erase, program, and verify the memory module of the MSP430 flash-based microcontroller family using the JTAG communication port.

    However this JTAG interface is not 100% IEEE 1149.1 (JTAG) compatible. For example none of the MSP430 devices has Boundary Scan Cells. We only support the required command BYPASS, but don’t support the other required commands for example EXTEST and SAMPLE/PRELOAD.

    Therefore there is no BSDL file for any MSP430 devices. In addition you can not put a MSP430 into a JTAG chain together with other devices.

    If this answers your question, please click "Verify it as the answer"
    Regards,
    Wade

     

  • Hi Wade,

    Got it, thanks for your help.

    LEON