Part Number: TPS74401-EP
Hi there,
Currently, i am developing an electronic system using the TPS74401-EP LDO.
The TPS74401-EP is used to drop a 3.3V main power to 1.2V Processor core power.
I expect that an output current of a 1.2V supply power is required approximately 2.2A.
If the development system operates at -40 to 125 ° C, will the chip break down?
(I calculated the allowable operating temperature as follows.
Top = Tj - Rjc(Junction to bottom case thermal resistance) x P
= 125° C - 2.4° C/W X 4.6W
= 113.96° C)
through the above calculations, I derived the operating temperature of 113° C. Is the above calculation correct?)
please answer my question.