This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/ADS5400-SP: Behavioral Model for ADS5400-SP

Part Number: ADS5400-SP

Tool/software: Linux

Hi,

I am working on a project where we use ADS5400-SP part on the board and our FPGA interface with ADS5400-SP. I am looking for behavioral model of ADS5400-SP wither in SystemVerilog or Verilog. My main work is verifying FPGA and would be helpful to have model from the same company that we purchase it from, so we have more confidence in verifying the FPGA that interfaces with ADS5400-SP along with other interfaces that our FPGA uses.

Thanks,

Ram