Hi Team,
One of my customer is using LT1014 and need confirmation on the max and min input which can feed to the device while operating at 5V Vcc. Is it possible to give -13V input to LT1014 powered from +5V Single supply. No ESD diodes are visible in block diagram, what will be the limiting factor and the damage to device if the input is lower or higer than Vcc.
Thanks in advance for your help and support.
Regards, Shinu Mathew.