This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3809-EP: Thermal Resistance

Part Number: TPS3809-EP

I need the thermal resistance information for the given part (TPS3809K33MDBVREP) with a unit of °C/W and for a junction to board, or junction to case preferred. Other acceptable information may be junction to ambient, or junction to lead. Thank you.

  • Hello Michael,

    We do not have these numbers currently available. I have began the process to model the package in order to get the values. This can take up to two weeks. I will update you as soon as I have them. In the meantime here is the dissipation ratings (you've likely already seen this from the datasheet).

    Thanks,

    Kyle

  • Hello Michael,

    Here are the obtained values based off of our device modeling. All are in C/W.

    Result- Theta JA-High K (standard datasheet value): 255.4
    Result-Theta JC, top (standard datasheet value): 155.4
    Result-Theta JB (standard datasheet value): 131.7
    Result- Psi JT (standard datasheet value): 51.8
    Result- Psi JB (standard datasheet value): 130.6

    Thanks,
    Kyle