This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 1
Views: 2076
Hi, I'm asking here because the OMAP3 forum seems to be no longer supported.
What is the maximum upload size for a boot image sent via USB peripheral boot, for the OMAP3630 in HS mode? For my target board it doesn't seem to accept an image greater than 28664 bytes - is this the limit? I'm curious because the 2nd boot file that is loaded from the MMC2 interface is more like 60kB in size, so I don't understand why the memory boot can copy a larger file into RAM than the peripheral boot can.
Thanks!
George
Hi,
We apologise that we could support only OMAPL13x, AM1x, C674x device related queries on this forum. So, I am moving back your post to OMAP35x forum to be better answered.
Thanks & regards, Sivaraj K