This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Unable to connect TI XDS100v3 to pandaboard_ES with CC Studio v 5.5.1 . (The JTAG DR Integrity scan-test has failed.)

Prodigy 50 points

Replies: 1

Views: 2311

Hi all,

I have purchased a TI XDS100v3 to debug pandaboard but i am unable to connect it . It says The JTAG DR Integrity scan-test has failed.

I will be very grateful to you for your HELP!!!!!


Execute the command:

%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity

[Result]


-----[Print the board config pathname(s)]------------------------------------

C:\Users\Echo\AppData\Local\.TI\4289855962\
0\0\BrdDat\testBoard.dat

-----[Print the reset-command software log-file]-----------------------------

This utility has selected a 100- or 510-class product.
This utility will load the adapter 'jioserdesusbv3.dll'.
The library build date was 'Aug 20 2013'.
The library build time was '22:56:19'.
The library package version is '5.1.232.0'.
The library component version is '35.34.40.0'.
The controller does not use a programmable FPGA.
The controller has a version number of '4' (0x00000004).
The controller has an insertion length of '0' (0x00000000).
This utility will attempt to reset the controller.
This utility has successfully reset the controller.

-----[Print the reset-command hardware log-file]-----------------------------

The scan-path will be reset by toggling the JTAG TRST signal.
The controller is the FTDI FT2232 with USB interface.
The link from controller to target is direct (without cable).
The software is configured for FTDI FT2232 features.
The controller cannot monitor the value on the EMU[0] pin.
The controller cannot monitor the value on the EMU[1] pin.
The controller cannot control the timing on output pins.
The controller cannot control the timing on input pins.
The scan-path link-delay has been set to exactly '0' (0x0000).

-----[The log-file for the JTAG TCLK output generated from the PLL]----------

Test Size Coord MHz Flag Result Description
~~~~ ~~~~ ~~~~~~~ ~~~~~~~~ ~~~~ ~~~~~~~~~~~ ~~~~~~~~~~~~~~~~~~~
1 512 - 01 00 500.0kHz O good value measure path length
2 512 + 00 00 1.000MHz [O] good value apply explicit tclk

There is no hardware for measuring the JTAG TCLK frequency.

In the scan-path tests:
The test length was 16384 bits.
The JTAG IR length was 6 bits.
The JTAG DR length was 1 bits.

The IR/DR scan-path tests used 2 frequencies.
The IR/DR scan-path tests used 500.0kHz as the initial frequency.
The IR/DR scan-path tests used 1.000MHz as the highest frequency.
The IR/DR scan-path tests used 1.000MHz as the final frequency.

-----[Measure the source and frequency of the final JTAG TCLKR input]--------

There is no hardware for measuring the JTAG TCLK frequency.

-----[Perform the standard path-length test on the JTAG IR and DR]-----------

This path-length test uses blocks of 512 32-bit words.

The test for the JTAG IR instruction path-length failed.
The JTAG IR instruction scan-path is stuck-at-ones.

The test for the JTAG DR bypass path-length succeeded.
The JTAG DR bypass path-length is 32 bits.

-----[Perform the Integrity scan-test on the JTAG IR]------------------------

This test will use blocks of 512 32-bit words.
This test will be applied just once.

Do a test using 0xFFFFFFFF.
Test 1 Word 0: scanned out 0xFFFFFFFF and scanned in 0xFFFFFFC1.
Scan tests: 1, skipped: 0, failed: 1
Do a test using 0x00000000.
Test 2 Word 0: scanned out 0x00000000 and scanned in 0x0000003F.
Scan tests: 2, skipped: 0, failed: 2
Do a test using 0xFE03E0E2.
Test 3 Word 0: scanned out 0xFE03E0E2 and scanned in 0x80F83880.
Test 3 Word 1: scanned out 0xFE03E0E2 and scanned in 0x80F838BF.
Test 3 Word 2: scanned out 0xFE03E0E2 and scanned in 0x80F838BF.
Test 3 Word 3: scanned out 0xFE03E0E2 and scanned in 0x80F838BF.
Test 3 Word 4: scanned out 0xFE03E0E2 and scanned in 0x80F838BF.
Test 3 Word 5: scanned out 0xFE03E0E2 and scanned in 0x80F838BF.
The details of the first 8 errors have been provided.
The utility will now report only the count of failed tests.
Scan tests: 3, skipped: 0, failed: 3
Do a test using 0x01FC1F1D.
Scan tests: 4, skipped: 0, failed: 4
Do a test using 0x5533CCAA.
Scan tests: 5, skipped: 0, failed: 5
Do a test using 0xAACC3355.
Scan tests: 6, skipped: 0, failed: 6
Some of the values were corrupted - 66.7 percent.

The JTAG IR Integrity scan-test has failed.

-----[Perform the Integrity scan-test on the JTAG DR]------------------------

This test will use blocks of 512 32-bit words.
This test will be applied just once.

Do a test using 0xFFFFFFFF.
Scan tests: 1, skipped: 0, failed: 0
Do a test using 0x00000000.
Scan tests: 2, skipped: 0, failed: 0
Do a test using 0xFE03E0E2.
Test 3 Word 0: scanned out 0xFE03E0E2 and scanned in 0xFC07C1C5.
Test 3 Word 1: scanned out 0xFE03E0E2 and scanned in 0xFC07C1C5.
Test 3 Word 2: scanned out 0xFE03E0E2 and scanned in 0xFC07C1C5.
Test 3 Word 3: scanned out 0xFE03E0E2 and scanned in 0xFC07C1C5.
Test 3 Word 4: scanned out 0xFE03E0E2 and scanned in 0xFC07C1C5.
Test 3 Word 5: scanned out 0xFE03E0E2 and scanned in 0xFC07C1C5.
Test 3 Word 6: scanned out 0xFE03E0E2 and scanned in 0xFC07C1C5.
Test 3 Word 7: scanned out 0xFE03E0E2 and scanned in 0xFC07C1C5.
The details of the first 8 errors have been provided.
The utility will now report only the count of failed tests.
Scan tests: 3, skipped: 0, failed: 1
Do a test using 0x01FC1F1D.
Scan tests: 4, skipped: 0, failed: 2
Do a test using 0x5533CCAA.
Scan tests: 5, skipped: 0, failed: 3
Do a test using 0xAACC3355.
Scan tests: 6, skipped: 0, failed: 4
Some of the values were corrupted - 66.7 percent.

The JTAG DR Integrity scan-test has failed.

[End]

1 Reply

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.