This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TDA2x 100Mbit Ethernet

Prodigy 50 points

Replies: 2

Views: 2800

Hi everbody,

i posted a picture from a tda2xx EVM.

My question is why they have the new release of the tda2xx evm this 100mbit sticker on the ethernet port?

Is there any problem with this ethernet port?

  • Hello Benedikt,

    There is a bug with RGMII module - RGMII2 (rgmii1_* signals) Switching Characteristics only support 10/100 Mbps operation. RGMII2 Switching Characteristics are not compatible with 1000 Mbps operation. Refer to the device Data Manual for Switching Characteristics timing details.

    See in TDA2x Errata document: Ethernet RGMII2 limited to 10/100 Mbps; Errata ID: i880

    The proposed workaround is: RGMII2 (rgmii1_* signals) should be used at 10/100 Mbps operation only. If 1000 Mbps operation is required, RGMII1 (rgmii0_* signals) can be used instead.

    Best regards,
    Yanko

      Please click the Verify Answer button on this post if it answers your question.

            Be sure to read the OMAP Application Processors Forum Guidelines and FAQ

  • In reply to Yanko Todorov-XID:

    Hello Benedikt,

    Please see the patch in Uboot - lists.denx.de/.../158269.html

    Best regards,
    Yanko

      Please click the Verify Answer button on this post if it answers your question.

            Be sure to read the OMAP Application Processors Forum Guidelines and FAQ

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.