hi
i'm tring to run an android application that use the front camera using TEVMXXX-CAM-V1-0 module.
if ii connect the camera to "camera 1" port i can refer it only as BACK camera, and when i connect the camera module to the "camera 2" port , the device dosn't recognizing the camera.
look for recognition by run camera_test f command on the adb shell screen.
is there any way to refer the camera as FRONT camera to have the mirroring effect ?