Hi all,
I am using tinycap to capture signals from 4 digital mics present in OMAP4460 Blaze tablet .
My tinycap settings are as follows.
tinycap /sdcard/test.pcm -D 0 -d 0 -c 4 -r 48000 -b 32 -p 768 -n 10
The data do get captured on four digital microphones but i see many audio losses in the captured signal.
1) What is the reason for the audio losses.
2) What si the maximum data size that can be allocated to store the captured data ( i.e. period_size * number_of_buffers * sizeof( WORD32) ).
3} how can i stop the Audio loss