Dear all, I am working with denx u-boot and PandaBoard.
I am trying to write a file to SD card in spl_mmc.c. During compilation gcc moans: undefined reference 'file_fat_write'. I don't understand why. Directly after the (original) code in mmc_load_image_fat(): err = file_fat_read(payloadname, (u8 *)spl_image.load_addr, 0); I insert the following code: file_fat_write("foo", "foo", 3); Why doesn't gcc know this function as it is also declared in include/fat.h just as file_fat_read() is? Did someone manage to write to fat out of the SPL? Best, André