Hi,
I have a requirement to backport SD card driver from TI omap3 linux 2.6.37 to TI omap3 linux 2.6.32.
Can any one help me what are the files I need to update for SD card whole driver?
i.e drivers/mmc/core/sd.c or any others?
I am using 4GB micro SD card.
And one more thing I have to print message in driver after 4096 bytes of data is read from SD card, for that at which location in file, I have to modify?
Thanks in advance for your efforts and time.
Regards,
Shital