Hi,
May I know what is the maximum current of BUZ_AC and BUZ_DC can be supplied to drive the buzzer ?
I face problem with my board that the BUZ_AC pin keep on generating the pulse signal with amplitude of about 150mV
even there is no receiver put on it. So I can hear the audible sound from the buzzer.
I used a mosfet to drive the buzzer instead of directly connect to the pin.
What is the purpose of 10K resistor connected from BUZ_AC to GND ?
I don't have this resistor in my design.
Thanks.