Hello Forum, is there a signal that I can use from the BQ51010B to indicate when it is on the charging pad?
That's all I need to know, that my wireless receiver product is on the pad.
I see this note in the data sheet.
The bq5105x provides one status output, CHG. This output is an open-drain NMOS device that is rated to 20 V.
The open-drain FET connected to the CHG pin will be turned on whenever the output (BAT) of the charger is
enabled. As a note, the output of the charger supply will not be enabled if the VRECT-REG does not converge to the
no-load target voltage.
Will CHG tell me I am on an active charging pad?
Thank you.