Hi,
What is the bq500511+bq50002 current consumption data?
I notice in bq500511 datasheet, active mode current is about 3.45mA, while low power mode current is about 285uA.
What are the use cases for active mode and low power mode?
When the Charging TX IC bq500511 is continuous pinging the RX device and nothing found for long time, is it still in lower power mode?
Does active mode meaning the actual charging from TX IC to RX IC is running?
If it is not in the charging status (i.e. long time search status), what is the total power consumption for bq500511+bq50002?
What is the time interval for every ping from bq500511 to RX device?
Since I want to use battery as Charging TX IC source instead of external DC, so current consumption is important.
Regards
Rongfeng