Hello all,
My questions are about the EVM of BQ51050B - the bq51050BEVM-764
i refer to the below datasheet of this component
http://www.ti.com/lit/ug/sluua25c/sluua25c.pdf
my questions are :
1) can it use other coil for Rx ?
2)what capacitors should be replaced for Rx tuning? C1,C2,C3? Is there a formula for that?
3) can I place 4 ohm (25 Watt) resistor as load? Instead of the Emulator depicted in the data sheet in Figure 3?
Thanks
Igor