Other Parts Discussed in Thread: ISO7741, ISO6741
How to connect SPI MCU to multiple isolated SPI nodes?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Digital isolators like ISO7741 and ISO6741 feature enable pins (ENx) which can be used to either enable or tri-state the respective outputs thereby allowing multiple output pins of multiple devices to be connected together. This enables an MCU with SPI interface to be connected to multiple other nodes with SPI interface while still maintaining isolation.
Please refer to the below diagram that shows how an MCU with SPI interface can be connected to multiple nodes through digital isolators. The MCU uses select lines to enable only one digital isolator at a time thereby allowing data from only one SPI node to be read at any point of time.