This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G17: Confirmation of thresshold

Part Number: SN74LVC1G17

HI,

When reading table 7.5 in data sheet, it shows for V(t+) of 3V supply that minimum is 1.48V and maximum is 1.92V.   I am writing to confirm the device will not transition for positive input until the input is at or above 1.48V and may take all the way to 1.92V before the logical transition takes effect.   Is this understanding correct?  If so then there is no possibility for an noisy input that is always below 1.48V (let us say 0.7V) to create an unintended transition.  Is this understanding correct?  Any further comments?   

Thank you,

HSG