Other Parts Discussed in Thread: TXU0304-Q1
Hello all,
If the level converter is used for an SPI interface, are series resistors required for EMC improvements?
And if so on both sides?
Best regards
Olaf
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello all,
If the level converter is used for an SPI interface, are series resistors required for EMC improvements?
And if so on both sides?
Best regards
Olaf
Hey Olaf,
Whether or not its required would likely depend on the system it goes in. I would also recommend using the TXU0304-Q1 device instead for SPI. I would place 0 ohm resistors on the outputs in case the outputs need to be dampened later on.