これは、SN74HCS72のスパイスモデルを使用してシミュレートされます。
/ CLKが10kΩで5Vにプルアップされると、/ CLKの電圧は約1.5Vまでしか上昇しません。
これは正しい動作ですか?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
これは、SN74HCS72のスパイスモデルを使用してシミュレートされます。
/ CLKが10kΩで5Vにプルアップされると、/ CLKの電圧は約1.5Vまでしか上昇しません。
これは正しい動作ですか?
Hello,
Ive translated this issue to the following :
This is simulated using the SN74HCS72 spice model.
When / CLK is pulled up to 5V with 10kΩ, the voltage of / CLK only rises to about 1.5V.
Is this the correct behavior?
I've assigned this to our modeling expert who will help you with this issue. Let me know if there is anything lost in the translation so we can better help you.
Thanks,
Rami
Hello,
There is an issue with the SPICE model. I have fixed the issue and reattached the model. Please let me know if you need any further help with this.
Regards,
Karan