Other Parts Discussed in Thread: SN74LV1T125,
I usually do 1.8V to 3.3V level shift using SN74LV1T125. I find there is a direction-controlled version, SN74AXC1T45. I wonder what's the benefit to use it, except the controllable direction?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I usually do 1.8V to 3.3V level shift using SN74LV1T125. I find there is a direction-controlled version, SN74AXC1T45. I wonder what's the benefit to use it, except the controllable direction?
Thanks.
The primary benefit is the dual-supply device (SN74AXC1T45) will use far less power than the reduced threshold single supply device (SN74LV1T125). It also allows more flexibility in routing because of the selectable direction -- most of our customers don't use the direction pin to switch directions, but to set the direction permanently.