Team,
We are using SN74LVC1G08DBVRE4 for one of our application. Below image is for reference of the circuit
Pin 1 - Pulled up - Will be HIGH always
Pin 2 - Will be high after some delay(12ms) with respect to a reference pulse
We are seeing a glitch at pin 4 of the AND gate as shown in the below image where as this is not seen at the inputs. GREEN waveform is our reference waveform.
IMAGE 1 - PIN 1(Yellow)
IMAGE 2 - PIN 2 (Yellow)
IMAGE 3 - PIN 4(OUTPUT) (Yellow)
Could you please help on the same.
BR,
Arun