Hi team,
Original I found CD4094B to replace HEF4094BT. But package different with HEF4094BT.
CD4094B: SO16
HEF4094BT:SOIC16
So, Does TI have like this package with HEF4094BT? thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
Original I found CD4094B to replace HEF4094BT. But package different with HEF4094BT.
CD4094B: SO16
HEF4094BT:SOIC16
So, Does TI have like this package with HEF4094BT? thanks!
Hello,
We don't have exactly the same package, however the NS package has the same pin pitch (1.27 mm) so these two different packages could be used on the same board just by changing the pad lengths slightly (increase length by ~2mm):
Nexperia package:
TI NS package:
Hi Emrys,
My customer thinks SOIC16 is a popular package.
So is it possible that as another P/N for the same package and function?
SOIC16 is a popular package, but it's not available for this device. CD4094B is unique in our portfolio -- we don't have any direct replacements.