This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC2G07: Higher abs max voltage

Part Number: SN74LVC2G07

Customer is using Buffer part # SN74LVC2G07DBVR in one of designs. This part output is tolerable to max of 6.5V per datasheet. They are looking for the buffer with below specifications.

 

  • Buffer output or open drain output shall be tolerable to voltage >7V (<10V whichever voltage part is available)
  • Rest of the specifications will be same as SN74LVC2G07DBVR
  • If required spec part is not available, please suggest Dual transistor with internal biasing resistor with same package and pins of SN74LVC2G07DBVR.

Any recommendations here?