Other Parts Discussed in Thread: TXU0304, SN74LVC3G17, TXB0106-Q1, TXB0104-Q1, TXS0104E-Q1
Hi Support Team,
1. My customer needs a Voltage translator to convert 5V to 3.3V.
5V is from MCU SPI.
2. www.ti.com/.../products.html
My customer seached voltage translator in the above link, my customer would like to know the following questions:
①There are two input types: transmission gate and CMOS. What is the difference?
②What is the difference between applications and technology family?
Can be used for SPI, why can't it be used for I2C?
Thanks so much.
Best regards,
Yuki