This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74HCS125: Input Threshold Voltage

Part Number: SN74HCS125
Other Parts Discussed in Thread: SN74LV4T125, SN74AHCT125, SN74AHCT541, SN74AHCT1G125, TXU0104

We're looking for the 4ch buffer with VCC=5V, and the Input Voltage is from MCU 3.3V. 

It looks SN74HCS125 is able to meet this requirement. But we'd like to double check with you the input threshold. 

in the d/s, it says:

In the application, the 3.3V input (+/-5% tolerance) is applied to the buffer. Is this input threshold able to meet? Is the design margin of the input voltage good enough? 

If it's not suited one, is there other device you suggest to use with this conditions?