From the detail data sheet, it show SN74HC14DR with "NIPDAU | SN" at the "Lead finish/ Ball material" column but SN74HC14DRG4 with "NIPDAU " at "Lead finish/ Ball material". Are both the same part?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
From the detail data sheet, it show SN74HC14DR with "NIPDAU | SN" at the "Lead finish/ Ball material" column but SN74HC14DRG4 with "NIPDAU " at "Lead finish/ Ball material". Are both the same part?
Footnote (6) says:
Orderable Devices may have multiple material finish options. Finish options are separated by a vertical ruled line.
The SN74HC14DR is made at multiple manufacturing sites, which use different lead finishes. Both tin and nickel/palladium/gold conform to the datasheet specifications.