This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LSF0101: Add on voltage translator LSF0101 for SN74LVC1G123

Part Number: LSF0101
Other Parts Discussed in Thread: SN74LVC1G123, SN74AXC1T45, SN74GTL2014, SN74AXC4T245, SN74AXC8T245

Hi, 

The output of  SN74LVC1G123 is level shifted by LSF0101.

The lowest Vref_A of LSF0101 is 0.95V in datasheet.

In the simulation, the Vref_A is divider to 0.763V from 3.3V and the output of A follow Vref_A supply, which is ~0.7V. 

Any mistake in the simulation or the datasheet spec?

Would it a problem if the Vref_A is smaller than the min of Vref_A (0.95V) ?