Other Parts Discussed in Thread: SN74AUP1G125, SN74AUC1G125, SN74AUC1G17
Is there any direct replacement for the SN74LV1T125 with VCC input of 1.6V?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is there any direct replacement for the SN74LV1T125 with VCC input of 1.6V?
Hi Jayson,
Depending on your application, the SN74AUP1G125 or SN74AUC1G125 might be a good replacement. Both are also '125 functions (buffer with 3-state output).
Hi Emrys.
Will use for MIPI-CSI Camera power Enable.
Can I use SN74AUP1G125 or SN74AUC1G125 as a direct replacement? due to the SN74LV1T125DCKR has no available stock now. Thanks
Yes. In this application, you could also use a plain buffer without /OE such as the SN74AUC1G17.