This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXS0102: Can I use this Level Shifter in CANbus? Does it work properly in CANbus speed?

Part Number: TXS0102
Other Parts Discussed in Thread: ISO1050, TXS0104E, SN74AXC2T245, ISO1044, ISO1042

Hello,

I want to use TXS0102 for level shifting from 1.8V (my CAN controller works at 1.8V) to 3.3V (TI ISO1050 CAN transceiver accepts at 3.3V) . 

Can TXS0102 work at the CANbus speed properly? I saw some demo boards which use TXS0104E level shifter for this translation in CANbus.

Which level shifter ( TXS0102 or TXS0104E) should I use for CANbus? 

Best Regards,