This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AUP1T34: 25MHz Clock 3.3V to 1.0V

Part Number: SN74AUP1T34
Other Parts Discussed in Thread: SN74AUC1G17

Hi Team,

Any concerns with using the SN74AUP1T34 as a level translator from 3.3V to 1.0V on a 25MHz clock?

We noticed that the max propagation delay could be >40ns (for 3.0V to 0.9V), which would be longer than the 25MHz clock period, so are there any other devices you'd recommend instead?

Thank you,

Joe