Does this level translator have any issues if same supply voltage is used on VCCA and VCCB? This is because I see one of inputs not pulled high inspite of its other side being high.
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Does this level translator have any issues if same supply voltage is used on VCCA and VCCB? This is because I see one of inputs not pulled high inspite of its other side being high.
Thanks!
The supply used on VCCA and VCCB is 3V.
On output of Bx there is a pull up resistor. This signal is held high and on Ax it is low which has no pull up. Adding pull up on Ax will solve the problem but its not a clean way of doing it.
So my question is
- is same value of supply voltage cause any issue?
- is the pull up on both side necessary?
What is the value of the DIR pins? Please show a schematic.
Please note that input pins do not output a voltage.
- DIR2 pin is pull high to VCCA.
- B2 signal is held high (it has pull up resistor)
The issue is A2 signal is low
A2 is an input, which means that it must be driven externally.
If you want the signal to be high in this case, you need a pull-up resistor at the input. (The pull-up resistor at the output is needed only if you want a high voltage while the device is disabled or powered off.)