Hello team,
My customer asked the any devices which have VLT with the function of SN74AUCH16374.
They want to set the input 1.5V and output 1.8V. Do we have any devices with these feature?
Best Regards,
Austin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello team,
My customer asked the any devices which have VLT with the function of SN74AUCH16374.
They want to set the input 1.5V and output 1.8V. Do we have any devices with these feature?
Best Regards,
Austin
Hi Austin,
Can you clarify what you mean by "VLT"? I'm not sure what you mean by this function.
VIH is 1.17 V, so this is possible.
Please note that the bus-hold inputs, for a high level, have a resistor between the pin and VCC, so a small current will flow into the 1.5 V device's output.
Hi Albert,
I just said voltage level translator. The customer want to generate different output by the one chip solution.
Austin,
Per Clemens suggestion, if all you are trying to do is do voltage translation from 1.5V to 1.8V, then the device you already have is capable of interpreting a 1.5V input and having the output driven to VCC, since the VIH(min) is 1.17V, 1.5V is a valid input for the device.
Best,
Michael