Hi TI-team
I have a question about input / output protection when the power of SN74LVC1G126-Q1 is turned off.
If a voltage is applied to the input terminal when VCC = 0V, will the IC be damaged?
The data sheet says "Ioff Supports live insertion, partial-power-down mode, and back drive protection"
I think it's okay because the application report (Logic in Live-Insertion Applications.) Says "Ioff protection circuitry ensures that no excessive current is drawn from or to an input, output, or combined I/O that is biased to a specified voltage while the device is powered down.".
However, I checked it just in case because the explanation of the data sheet only mentions "This device includes circuitry to disable all outputs when the supply pin is held at 0 V. When disabled, the outputs will neither source nor sink current, regardless of the input voltages applied." (because the protection of the input terminal is not specified).
Best Regards,
Takuya Nagasawa