Other Parts Discussed in Thread: SN74LV541A
Hi Team, Seeking your inputs.
The PSpice model for the SN74LVC541A Octal Buffer contains a subcircuit (LOGIC_TRI_STATE_OUTPUT_LVC_1i_AND_Tristate_CMOS_SN74LVC541A IN OUT OEZ VCC VEE) which has two votage-controlled voltage sources; EROH and EROL. These sources are controlled by look up tables. However, the table entries contain two outputs for a 3 volt argument (see below). If you examine the similar SN74LV541A model you'll see only one 3 volt entry in that subcircuit.
EROH NROH VEE TABLE {V(VCC,VEE)} =
+(1.65,112.5)
+(2.3,50)
+(3,37.5)
+(3,29.1666666666667)
+(4.5,21.875)
EROL NROL VEE TABLE {V(VCC,VEE)} =
+(1.65,112.5)
+(2.3,37.5)
+(3,25)
+(3,22.9166666666667)
+(4.5,17.1875)
Thank you very much.
-Mark