Part Number: SN74AUP1T34
Other Parts Discussed in Thread: SN74LVC1G17, SN74AUC1G17, SN74AUP1G17, SN74AUP1G34, SN74LV1T34, SN74LVC1G34,
Hi,
The related thread stated:
"For down-converting, you can use the SN74LV1T34, or any buffer with an overvoltage-tolerant input, e.g., SN74LVC1G34, SN74AUP1G34, SN74LVC1G17, SN74AUP1G17, SN74AUC1G17.
For up-converting, you can use the SN74LV1T34."
But the SN74AUP1T34 seems to be the rare device that has power supplies on both Pins 1 and 5 (for the TSSOP-5 DCK package).
Is it OK to put the aforementioned buffers on the same footprint - i.e to supply power to the Buffer NC Pin 1?
I would like to use the alternative devices but without re-spinning the PCB.
Cheers,
Jack