This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G240: Vcc =5V power supply, power down the current is bigger, about 5mA

Part Number: SN74LVC1G240
Other Parts Discussed in Thread: SN74LXC2T45, SN74LV1T125, SN74LV1T04

Hi ,

control signal pin1 & pin2 is 3.3V, when Vcc =5V, pin1 is pulled 3.3V (off ) ,the current is high, about 5mA; did some test, i found that it is normal when Vcc is lower than 3.6V , when Vcc is more than 3.6V , the issue comes out; the schematic is as below,