Hi.
I am looking for the FIT rate of the part number with a 70% or higher confidence level.
Regards
Rekha Mohandas
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi.
I am looking for the FIT rate of the part number with a 70% or higher confidence level.
Regards
Rekha Mohandas
Hi Rekha,
These can be calculated from the existing FIT data on our website using the explanation in this application report: Calculating FIT for a Mission Profile
-
To save you time, I went ahead and calculated the values:
Confidence | FIT Rate |
60% | 0.5 |
70% | 0.6 |
80% | 0.8 |
90% | 1.2 |
95% | 1.5 |
99% | 2.3 |