This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AXC4T774: SN74AXC4T774BQBR IO protection

Part Number: SN74AXC4T774


SN74AXC4T774BQBR IO protection

Will the SN74AXC4T774BQBR be damaged if i will work at the next scenario:

1)VCCB = 3.3V

2)VCCA = 1.8V

3)OE pin connected to GND through 10kOhm resistor.

4)B1- Input on VCCB side

5)A1- Output on VCCA side

6)DIR1 connected to GND (signal from B1 to A1)

The scenario- if i don't assert any signal at B1 side, but i'm forcing 'H' logic on A1 side does the IC will be damaged?