Hi Team,
Do we have IC internal RC value can be information? Thank you.
Regards,
Roy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Roy,
I'm afraid I don't understand - what resistor or capacitor values are you trying to determine?
Hi Emrys,
Now, we are using B-> A direction. And we want to know below RC input. (red arrow)

Roy
Hi Roy,
With B set as an input, we would expect the capacitance to be between 1 and 10pF, with the typical value being 3pF.
The leakage current is up to 5μA at 6V, so the worst case 'resistance' to VCC and ground can be modelled as 1.2MΩ. For typical performance, I would recommend to use 120MΩ.