Hi expert,
For SN74LVC1G07-Q1, what's the output status when Vcc=0V, and input is LOW? Is there any internal pull-down resistance at the output pin? If yes, what's the value? Thanks.
Arie
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi expert,
For SN74LVC1G07-Q1, what's the output status when Vcc=0V, and input is LOW? Is there any internal pull-down resistance at the output pin? If yes, what's the value? Thanks.
Arie
Hi Arie,
This device has a partial power down feature, if the supply is at 0V then the input and output will enter a high impedance state. If you want to calculate the worst-case output resistance it can be derived from the VOL specifications: ROL = VOL / IOL
Sebastian