This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXS0108E-Q1: push pull and open drain

Part Number: TXS0108E-Q1

Hi Expert,

I have some questions about TXS0108E-Q1 push pull and open drain.

  • As you can see as below in datasheet, does this data rate apply to both TXS0108E-q1 input port and output port? If the input signal is push pull/open drain, TXS0108E-q1 can accept up to 100Mbps/1.2Mbps. Likewise,  If the output signal is push pull/open drain, TXS0108E-q1 can transmits up to 100Mbps/1.2Mbps. Is it right? And I also don't understand why there are two different data rate. What limits the rate? The interface's own feature?

  • I see that TXS0108E-q1 has internal pull up resistor about 4k ohm. If the signal path is MCU1(i2C)-->TXS0108E-q1-->MCU2(i2c), do I need pull up external resistor for both side? From my understanding, I don't need since we have internal pull up resistor.

Thanks a lot for help!

BR,

Elec Cheng