Other Parts Discussed in Thread: SN74AHC1G125, SN74LVC1G17, SN74AUP1G17
Hello,
I have an issue with a 50MHz clock (amplitude jitter).
The issue can be fixed by adding a buffer to the clock signal.
We used SN74AXC1T45DCKR for testing, but it is out of stock.
Can someone make a recommendation for an alternative part? It is a 3.3V signal, we need non-inverting and single channel.
There are so many options, I am having trouble choosing the right one.
SOT-23 package is preferred.