This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74HC595: /OE Pin Pull-up Resistor

Part Number: SN74HC595

Hi team,

What is the recommended pull-up resistor at /OE pin to pull it up to VCC during power-up to avoid potential glitch? How to calculate/estimate pull-up resistor? 

Use case:

  • VCC = 3.3V
  • 4x SN74HC595 sharing the same /OE bus, pulling-up by the same resistor to VCC. 
  • Currently using 10kohm and observed output glitch during VCC power up. 

I believe this is due to during power-up, /OE is slightly slower than VCC, and momentarily /OE is < 0.7*VCC, causing /OE is logic '0' for a short period time during power, resulting in unexpected output observed.