Other Parts Discussed in Thread: TXB0108
Hi Team
I need a level translator to translate 1.5V signals to 1.8V, for this purpose I choose PN: SN74GTL2003PW
1) for this part what is the minimum voltage at the lower side(Sn) to get 1.8V at the higher side(Dn)? will this work for 1.5V on Sn and 1.8V on Dn
2) What are the default input and output states of the IOs on both sides on power up and power down conditions?
3) Do I need to connect pull-up resistors on both (Sn and Dn) input and output sides?
4) What should be the value of pull-up resistors on IOs?
Thanks
Santosh