Other Parts Discussed in Thread: SN74LVC125A, SN74AUC17, SN74LVC125A-Q1, SN74LVC126A-Q1
Hello Team,
I am using an audio interface with I2S signals.
The MCU will be operating in 3.3V logic and the audio amplifier is in 1.8V logic.
1). Is the level translator CAXC4T774QBQBRQ1 a good choice for my application?.
2). Do I really need a bidirectional voltage translator to communicate with the audio amplifier?.
3). I have a pin shortage in the MCU. So can I pull up or pull down the direction control pins?
4). The pin description for the I2S audio amplifier I am using says they are input only. So I hope I can pull those direction control pins to low or high to enable the communication only in one direction.
Please correct me if I am wrong